Networks
The DC Twins
27. February 2024
The DC Twins
The electricity war between direct and alternating current was actually already decided in 1890. But after more than 130 years, the loser is gaining new significance. Dr. Martin Wetter and…
Lubmin – the energy community
22. November 2023
Lubmin – the energy community
With over 2,000 inhabitants, the title of seaside resort, miles of sandy beaches on the German Baltic Sea coast and a wildly eventful energy history with plenty of ups and…
Tiny houses under electricity
20. December 2021
Tiny houses under electricity
They are gray, they are inconspicuous, they are everywhere – and when it comes to electricity, nothing works without them. There are around 600,000 transformer or local network stations in…
The Lords of Lightning
29. November 2021
The Lords of Lightning
When these colleagues get going, local public utilities have to put in extra shifts. Trabtech’s lightning protection laboratory enjoys a legendary reputation and is home to countless developments that protect…
Energy on all levels
9. November 2020
Energy on all levels
When walking through the plant, there is a constant crackling noise above. And the warnings are still ringing in our ears: Always take small steps. Do not raise your arms…
What does INGO do?
4. November 2020
What does INGO do?
INGO is small, rectangular and very red. And it is useful. Because renewable energies can be so exhausting. They make completely new demands on the finely balanced system of the power…
Always nice and bright
30. October 2020
Always nice and bright
The sun is shining when Christoph Werlitz opens the gates to the Menteroda solar park. It’s weather that’s appropriate for a visit to a plant that produces clean energy in…
Who invented it?
14. February 2020
Who invented it?
With the combined protection and field control device KOMBISAVE, the developers of the Swiss Phoenix Contact subsidiary NSE have hit the bull’s eye. Even though this should be avoided if…
IRMA keeps watch
13. February 2020
IRMA keeps watch
Big Brother is watching you. Even more so if it’s actually a member of your own family and not an unknown intruder. The public utilities in Bad Pyrmont therefore tend…