Provider

Lubmin – the energy community

Lubmin – the energy community

With over 2,000 inhabitants, the title of seaside resort, miles of sandy beaches on the German Baltic Sea coast and a wildly eventful energy history with plenty of ups and…
Tiny houses under electricity

Tiny houses under electricity

They are gray, they are inconspicuous, they are everywhere – and when it comes to electricity, nothing works without them. There are around 600,000 transformer or local network stations in…
It does not work without Chile

It does not work without Chile

The vision of an All Electric Society, in which fossil fuels are replaced by intelligently networked regenerative energy generation, cannot be realized without Chile. Chile is the world’s largest copper…
Fitness for the water pipeline

Fitness for the water pipeline

Water is a foodstuff. When it comes out of the tap, it’s even very inexpensive, as it costs an average of just 0.2 cents per liter. But there is another…
Power to Pressure

Power to Pressure

When the only compressed air energy storage and gas turbine power station in Europe went into operation in Huntorf, Germany, in 1978, an energy revolution towards renewables had not even…
Who invented it?

Who invented it?

With the combined protection and field control device KOMBISAVE, the developers of the Swiss Phoenix Contact subsidiary NSE have hit the bull’s eye. Even though this should be avoided if…
IRMA keeps watch

IRMA keeps watch

Big Brother is watching you. Even more so if it’s actually a member of your own family and not an unknown intruder. The public utilities in Bad Pyrmont therefore tend…
Back to top button